Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the H464AWK, series F6? (may be shown as F06)
Issue:
Product design repair parts

Product Line:
Heavy Duty Safety Switch

Resolution:
The repair parts for the H464AWK, series F6 (F06) are as follows. No other parts are available.
Complete Line Base - 4056703750 (1 required; includes phynolic base, arc suppressors, copper lugs, rotor, switching blades, and fuse clips)
NOTE: If using aluminum wire, replace lugs on line base with Al/Cu lug, 4025136550
Line Base mounting screws - 4020506501 (12 required per line base)
Load Base Assembly - 4056677450 (1 required per phase; includes phynolic base, lugs, and fuse clips)
Load Base mounting screws - 4020506501 (2 required per load base)
Arc Suppressor Assembly - 4056677550 (1 required per phase)
Arc Suppressor mounting screw - 4020514501 (1 required per arc suppressor assembly)
Lug Assembly - 4025136550 (1 required per phase)
Lug Assembly mounting screw - 2140122240 (per lug)
Switch Mechanism - 4056740150 (also requires interlock shaft gasket 4056786001)
Switch Mechanism mounting screws- 2299940562 (2 required)
Handle Assembly - 4056746850 (requires handle gasket 4056603101)
Lockplate - 4056746701
Lockplate mounting screws - 2299940562 (2 required)
Ground Lugs - 4025101652 (per lug)
Ground lug mounting screw - 4020513503 (per lug)

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings