Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can 100% rated breakers be installed in a Main lug only or MB I-line panel?
Issue:
Will I-line panels both MLO and MB panels accept 100 percent rated breakers?

Product Line:
Panels and breakers

Environment:
I- line panels and I-line breakers

Resolution:
Yes they can. However, the panel will still need to be protected by an upstream SCP device unless the 6 disconnect rule is applied.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings