Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What does suffix 6141 indicate on a circuit breaker?

Issue:
6141 indication

Product Line:
Molded Case Circuit Breaker

Environment:
Legacy Circuit Breaker

Resolution:
The 6141 suffix indicates a special magnetic calibration of hold 3500 A, trip 4000 A.

This means the breaker will hold on a short circuit of less than 3500 A, trip at a short circuit of greater than 4000 A, and it with either hold or trip in between 3500 - 4000 A.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings