Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Do Schneider Electric Low voltage transformers come with a ground bar?
Issue:
Are ground lugs, ground bars, or ground terminals included with the low voltage transformers?

Product Line:
Transformers

Environment:
EE, EX, EXN Seald resin, epoxy encapsulated

Resolution:
Our Transformers do not come with ground bars, lugs, or terminals. The design of the
enclosure base includes three locations for mounting a ground terminal bar but those are provided by others OR, you can use the lugs from our secondary DASK lug kits. Those include a ground lug..

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings