Issue:
What is the part number for the primary main and secondary main breakers used in the MPZB15T2F25K?
Product Line:
Mini Power zone
Environment:
MPZB15T2F25K
Resolution:
The primary main breaker for the MPZB15T2F25K is FHL36040 and the Secondary main is QOB360. These breakers may NOT be changed to different ampere ratings. Doing so will void the UL listing and any remaining warranty on the mini powerzone.
What is the part number for the primary main and secondary main breakers used in the MPZB15T2F25K?
Product Line:
Mini Power zone
Environment:
MPZB15T2F25K
Resolution:
The primary main breaker for the MPZB15T2F25K is FHL36040 and the Secondary main is QOB360. These breakers may NOT be changed to different ampere ratings. Doing so will void the UL listing and any remaining warranty on the mini powerzone.
Released for: Schneider Electric USA