Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can motor operators fit and work for the 4 pole PowerPacT L-frame breakers?
Yes, they will fit and work similar to the PowerPacT L-frame 3 pole breakers because the cover of the 4 pole is split into 3 poles + 1 pole. The 3 pole section is where the motor operator will mount. See attached photo below:
Pic showing cover split between 3 poles and neutral pole

Schneider Electric USA

Attachment(s)
LJL46600U31X-STANDARD.jpg [18.7 KB]
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings