Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Is there a vibration/shock rating for the Powerpact B-frame breakers?
Product Line:
Circuit Breakers

Resolution:
PowerPact B-frame devices resist mechanical vibrations.

They meet following levels of IEC 60068-2-6:
• 2.0 to 25 Hz and amplitude ±1.6 mm.
• 25 to 100 Hz acceleration ±4 g.

Note: Excessive vibration may cause tripping, breaks in connections, or damage to mechanical parts.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings