Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for a QMB3640?

Issue:
What are the repair parts for a QMB3640?

Product Line:
QMB panelboard, switchboard with QMB distribution

Resolution:
The QMB3640, series 4 switch and any associated parts are no longer available. Depending upon the age and style of the panel, the QMB3400LA might be a suitable replacement. If the panel is a QM style panel made before 1961, there would be no replacement available. If the panel is a QM style panel made between 1961 and 1984, the QMB3400LA will work as a replacement. If the panel is a QW style, then the QMB3400LA will work as a replacement with the addition of the QMB310EX plug on extension assembly. For further explanation, see attached document.

NOTE: The QMB3400LA will only have 42 kAIC @ 240 V, 30 kAIC @ 480 V, 22 kAIC @ 600 V.

Schneider Electric USA

Attachment(s)
QMB Replacements.pdf [141.96 KB]
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings