Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the maximum 3 pole QOB breaker available?
Issue:
What is the maximum amperage rating available for a 3-pole QOB breaker?

Product Line:
Miniature Circuit Breakers

Resolution:
100 A for QOB breakers. QOB-VH (22 kAIC) breakers are available up to 150 A. The 110, 125, and 150 A breakers require 6 pole spaces, all on the same side.

Schneider Electric USA
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
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Tech Support: 877-342-5173
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Software and Firmware
  • Product Selector
  • Product Replacement
  • DigestPLUS Online Catalogue
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings