Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the difference between "old style" EZM meter centers and "new style"?
Issue:
How are the old and new style EZM device bus bar styles different?

Product Line:
Metering Equipment

Resolution:
The old style EZM used a horizontal stacked (front to rear) bus structure provided with a sliding joint-pack and single VISI-TITE joint bolt for connecting the main bus cabinet to cabinet. The new style EZM is configured with a horizontal bus structure placing each bus bar one above the other for connecting the main bus cabinet to cabinet.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings