Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can a branch breaker larger than 100A be installed in the obsolete NH1B panelboard?
Issue:
What is the maximum branch circuit breaker that can be installed in the obsolete NH1B panelboard?

Product Line:
Obsolete NH1B circuit breaker panelboards.

Enviroment:
Obsolete NH1B panelboards sold and supported in the USA.

Cause:
Selection of branch circuit breakers for the obsolete NH1B panelboard.

Resolution:
The NH1B panelboard is limited to 100 amp maximum, F frame branches.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings