Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can an MP Meter-Pak meter center be series rated with an upstream device?
Issue:
Product Design

Product Line:
MP Meter Pak

Resolution:
No. The MP Meter-Pak meter centers are UL listed as "Suitable ONLY for use Service Equipment" and cannot be used downstream from any type of disconnect. Each Meter-Pak device has its own short circuit current ratings based on the tenant breakers used for the device.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings