Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can Transformers be used to change voltages in amounts greater than shown in the Buck & Boost literature?
Issue:
Buck and Boost Transformers have a limited voltage range

Product Line:
LV Transformers

Environment:
Applies to Resin Epoxy Encapsulated Transformers by SquareD/Schneider Electric


Cause:
Wider ranges of voltages may have to be increased or decreased than Buck and Boost Transformers can handle

Resolution:
Yes, standard single phase lighting Transformers can be used in Autotransformer wiring configurations to achieve much greater voltage changes than available with Buck & Boost Transformers. Contact your local SquareD/Schenider Electric Sales Office for further assistance.  Or see pages 19-21 of  below attachment for more information.


Schneider Electric USA

Attachment(s)
Resin White Book.pdf [832.93 KB]
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings