Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Is there any way to get a 120 volt neutral connection on a 240 delta secondary?
Issue:
Center Tapped Secondaries

Product Line:
LV Transformers

Environment:
Applies to Low Voltage Transformers by SquareD/Schneider Electric

Cause:
Center Tapped Secondaries

Resolution:

There are no provisions for a neutral, or center tapped winding, connection on the delta winding. It must be ordered as a center tapped delta secondary (ex. EXN75T6HCT where the CT denotes a ``Center Tap``)
Warning: The capacity of the center tap of the secondary is limited to 5% of the nameplate kVA capacity of the Transformer (ex. on the EXN75T6HCT, nameplate is 75kVA, thus 75,000*.05=3,750VA or 3.75kVA at 120volts, or only 31.25 amps)


Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings