Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
How do I order an elapsed time meter for a Class 8536 starter in a NEMA 4X enclosure?
Issue:
What is the form used for an elapsed time meter of Type S Starters in NEMA 4X enclosure?

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
Type S Contactors and Starters

Resolution:
With a NEMA 4X enclosure an elapsed time meter has to be internally mounted because the ETM is not NEMA 4X rated. Use form G107.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings