Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are handle blocking devices available for HOM circuit breakers?
Issue:
Are handle blocking devices available for HOM circuit breakers?

Product Line:
HOM 1p and 2p circuit breakers

Resolution:
These handle clamps/blocking devices will work on standard HOM breakers as well as GFI, EPD, CAFI, DF, PCAFI, and PDF breakers. They do not work on tandem or quad tandem breakers.
QO1LO:  Handle clamp for holding handle of HOM 1P in the ON or OFF position
HOM2HBD:  Handle blocking device for holding handle of HOM 2P circuit breakers in the OFF position

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings