Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the temperature rating on QO circuit breaker terminations?
Issue:
Temperature for QO breaker

Product Line:
Miniture Circuit Breaker

Resolution:
10-30 A breakers can use 60 or 75°C conductors.
35-150 A breakers can use 75°C conductors.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings