Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for a QMB364, Series D2 (D02)?
Issue:
What are the available replacement parts for QMB364, Series D2 (D02)?

Product Line:
QMB Switches

Resolution:
Only the parts listed below are considered field replaceable:
Arc Suppressor Assembly - 4052028950 (3 required)
Load Base Assembly - 4052002550 (3 required; includes lugs)
Load Base Mounting Screw - 4020506501 (2 required per load base)
Load Base Side Insulator - 4052025201 (1 required per load base)
Handle Knob Kit - 4028343650
Lug Assembly - 4025116251
Lug Mounting Nut - 2342702200

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings