Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for a QMB366W, Series E1 (E01) or Series E2 (E02)?
Issue:
Current design repair parts

Product Line:
Fusible QMB Switches

Resolution:
Only the parts listed below are considered field replaceable:
Complete Arc Suppression Assembly - 4052031850 and 4052085601 (3 required each)
Load Base Assembly - 4052112050 (3 required per switch, includes lugs)
Load Base Mounting Screw - 2142720241 (3 required per load base)
Load Base Side Insulator - 4052050850 (1 required per load base)
Fuse Clamp Assembly per phase - line side - 4052031351 (2 bolts included)
Fuse Clamp Assembly per phase - load side - 4052031350 (2 bolts included)
Handle Knob Kit - 4028343550
Lug Assembly - 4025128750 (per lug)
Lug Mounting Nut - 2342702400 (per lug)

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings