Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are double hole lugs available for the LA/LH style breakers?
Issue:
Is there a double-hole lug available for legacy L frame breakers?

Product Line:
Circuit Breakers

Resolution:
No, the standard lug is UL listed for two cables up to 250 kcmil under the single hole.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings