Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the optional lug kit for LA, Q4, and LH breakers?
Issue:
What is the alternate lug for LA, Q4, and LH circuit breakers?

Product Line:
Legacy MCCB

Resolution:
An optional lug is an AL400LH7, which accepts (1) 350 to 750 kcmil Al/Cu wire per phase. Compression and PDC (Power Distribution Connector) lugs are also available. See attached catalog pages.

Schneider Electric USA

Attachment(s)
Legacy Lugs.pdf [96.4 KB]
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings