Issue:
What are the available replacement parts for CU12L400L, series M01?
Product Line:
Combination Service Entrance Devices
Resolution:
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED BELOW.
The parts listed here are the only field replaceable parts that are still available:
What are the available replacement parts for CU12L400L, series M01?
Product Line:
Combination Service Entrance Devices
Resolution:
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED BELOW.
The parts listed here are the only field replaceable parts that are still available:
- Meter Cover - 4056151501
- Load Center Cover - 4056136152
- Dead Front Cover - 4056153701
- Mounting Channel - 4056142003
Released for: Schneider Electric USA