Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Will the 9001 K56YM work with a 1 5/8 inch mushroom knob?
Issue:
Checking if the 9001K56YM will work with a 1 5/8 in mushroom knob

Product Line:
Push Buttons and Operator Interface

Environment:
9001 Type K Push Buttons

Resolution:
Yes. It will work with the 1 5/8 inch and 1 3/8 inch.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings