Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for an MP66125, Series M01 branch unit?
Issue:
Current design repair parts

Product Line:
Meter Pak Metering

Resolution:
Only the parts listed below are considered field replaceable:
Customer Cover for one position (includes labels) - MP6125C
Circuit Breaker RB Cover (one position) - BCV
Cover Screws - 4020513002K
Meter Socket Cover (ring type, one position) - MMC
Meter Socket Sealing Ring (aluminum latch type) - 2920910001
Pull Box Cover - MM56125PC
Line Phase and Neutral Lugs - MMLK250
Alternate Lug Kits - Refer to Digest
Load Neutral and Service Ground Lug Assembly - 7329819862 (2 assemblies per device, one for the left side meter sockets and one for the right side meter sockets) each assembly has 5-lugs and the main neutral bus bar.
Mounting Screws for EACH Load Neutral/Service Ground Assembly:
(1) 2142720241 (mounts the assembly at the top to the Main Neutral bar of the device)
(1) 2149020120 (mounts the assembly to the enclosure just below the Main neutral bar connection)
(1) 2153217161 (mounts the assembly to the bracket at the back of the enclosure at the bottom of the assembly)

Equipment Ground Lug Assembly - 7329897052 (assembly includes 3 lugs and mounting bracket; 2 required per device, one for each set of meter sockets)
Mounting screws for EACH Equipment Ground Lug assembly - 2142217101 (2 per assembly)
Parts Kit (one position, meter socket line side through tenant breaker base) - MM125KIT
Mounting Channel - 7329652101

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings