Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for an MPR66125, Series M01 branch unit?
Issue:
Current design repair parts

Product Line:
Meter Pak Metering

Resolution:
Only the parts listed below are considered field replaceable:
Customer Cover for one position - MP6125C (includes labels)
Circuit Breaker RB Cover (one position) - BCV
Cover Screws - 4020513002K
Meter Socket Cover (ringless type, one position) - MMRC
Pull Box Cover - MP56125PC
Line Phase and Neutral Lugs - MMLK250
Alternate Lug Kits - Refer to Digest
Load Neutral and Service Ground Lugs Assembly: (2) 7329819862 (includes connector and 5 lugs; used on the LEFT and RIGHT side of the pull box)
Mounting Screws: 2153217161, 2142720240 and 2149020120 (1 each required per assembly)
Equipment Ground Lugs Assembly: 7329897052 (includes L-Bracket and 3 lugs; used on the LEFT and RIGHT side of the pull box)
Mounting Screws: (4) 2142217101 (2 required per assembly)
Parts Kit (one position, meter socket line side through tenant breaker base) - MM125KIT
Mounting Channel - 7329652101

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings