Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for an MP43200, Series M01 branch unit?
Issue:
Current design repair parts

Product Line:
Meter Pak Metering

Resolution:
Only the parts listed below are considered field replaceable:
Customer Cover (includes labels) - MP3200C
Circuit Breaker RB Cover (one position) - BCV
Cover Screws - 4020513002K
Meter Socket Cover (ring type, one position) - MMC
Meter Socket Sealing Ring (aluminum latch type) - 2920910001
Pull Box Cover - MP23200PC
Line Phase and Neutral Lugs - MMLK250
Alternate Lug Kits - Refer to Digest
Load Neutral and Service Ground Lug Assembly - 7329704351 (includes 5 lugs and bus bar the lugs mount on)
Mounting Screws for Load Neutra/Service Ground Assembly:
(1) 2142720163 (mounts the right side of the assembly to the Main Neutral bus bar)
(1) 2142717120 (mounts the left side of the assembly to the enclosure)

Equipment Ground Lug Assembly -  7329704451 (includes 3 lugs and the mounting bracket)
Mounting screws for the Equipment Ground Assembly - 2142217101 (2 required)
Parts Kit (one position, meter socket line side through tenant breaker base) - MP200KIT
Mounting Channel - 7329652001

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings