Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Which poles of a DC MP style Masterpact breaker are protected?
Issue:
Which poles of the MP Masterpact DC breaker have protection?

Product Line:
MP Style Masterpact Breakers

Resolution:
Poles 1 and 3 (from the left when looking at the breaker from the front) contain trip mechanisms. However, since the poles are always connected in series, the entire breaker and circuit has protection.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings