Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can ground fault detection be added to an F frame breaker in the field?
Issue:
Field installable ground fault module for the FA or FAL circuit breaker.

Product Line:
Molded Case Circuit Breaker

Resolution:
FA breakers must have a suffix G to be fit with a GFM100FA in the field to provide ground fault protection from 20 A -100 A.
If the breaker does not come with a G suffix, then the ground fault module cannot be field installed.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings