Issue:
What is the Handle Clamp for a QO breaker?
Product Line:
Miniature Circuit Breaker
Resolution:
There are 2 handle clamps available for QO breakers.
- For 1p QO breakers, the QO1LO handle clamp can hold the handle in the ON or OFF position.
- For 1, 2, or 3p QO or Q1 breakers, the HLO1 handle clamp can hold the handle in the ON or OFF position.
Both accessories are compatible with standard, CAFI, EPD, and GFI QO breakers,
Note: The clamp will not fit over the LED handle of the new AF/AFGF breakers. The only option for AF/AFGF breakers is the padlock attachment QOADV1PAF.
Released for: Schneider Electric USA