Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the operating temperature range of the UL489 listed Multi 9 breaker?
Issue:
What range of temperature are the UL489 listed Multi-9 breakers rated to operate at?

Product Line:
Multi9 Circuit Breakers

Resolution:
Range of operating temperatures is -30°C to +70°C.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings