Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is a 9001 AS1?
Issue:
What are the parts included in a 9001AS1?

Product Line:
Push Buttons and Operator Interface

Environment:
9001 K Selector Switches

Resolution:
This is a member of the Point of Purchase, or POP, system. These are devices packaged in plastic clam shells to display on a peg board at a distributor. The 9001 AS1 consists of a 9001 KS11BH13 and a 9001 KN244.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings