Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Is an IEC 947-3 rated automatic switch available in the Masterpact NW frame?
Issue:
Is there an IEC rated automatic switch available in the NW frame?

Product Line:
Masterpact NW Switches

Resolution:
Yes. An automatic switch is available with UL 489 and IEC 947-3 listings.
A non-automatic switch is available with ANSI C37 certification, UL 1066 Listing, and with IEC 947-3 listing.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings