Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the UL flame rating for the Multi-9 breakers?
Issue:
What is the UL flame rating for the Multi-9 breakers?

Product Line:
Multi-9 Breakers

Resolution:
The C60N UL1077, UL489A, and UL489 are V2 according to UL94.
The NC100H UL1077 is V0 according to UL94.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings