Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for an MP85200, Series M01 branch unit?
Issue:
Current Design repair parts

Product Line:
Meter Pak Metering

Resolution:
Only the parts listed below are considered field replaceable:
Customer Cover, Left Side (includes labels) - MP5200LC
Customer Cover, Right Side (includes labels) - MP5200RC
Circuit Breaker RB Cover (one position) - BCV
Cover Screws - 4020513002K
Meter Socket Cover (ring type, one position) - MMC
Blank Meter Socket Cover - MMCBK
Meter Socket Sealing Ring (aluminum latch type) - 2920910001
Pull Box Cover - MP56200PC
Line Phase and Neutral Lugs - MMLK500
LEFT Meter Sockets Load Neutral and Service Ground Lug Assembly - 7329704352 (includes 4 lugs and neutral bus bar the lugs are mounted on)
RIGHT Meter Sockets Load Neutral and Service Ground Lug Assembly - 7329704353 (includes 3 lugs and neutral bus bar the lugs are mounted on)
Mounting Screws for both Load Neutral/Service Ground Lug Assembly:
(1) - 2142720163 (mounts the right side of the LEFT assembly to the main neutral bar of the device)
(3) - 2142717120 (1 screw mounts the left side of the LEFT assembly to the enclosure and 2 screws mounts the RIGHT assembly to the main neutral bar and enclosure)
LEFT Meter Sockets Equipment Ground Lug Assembly - 7329704452 (includes 2 lugs and mounting bracket)
RIGHT Meter Sockets Equipment Ground Lug Assembly - 7329704451 (includes 3 lugs and mounting bracket)
Mounting Screws for BOTH Equipment Ground Lug Assembly - 2142217101 (2 required per assembly)
Parts Kit (one position, meter socket line side through tenant breaker base) - MP200KIT
Mounting Channel - 7329652101

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings