Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for an MPR86200, Series M01 branch unit?
Issue:
Current design repair parts

Product Line:
Meter Pak Metering

Resolution:
Only the parts listed below are considered field replaceable:
Customer Covers (includes labels) - (2) MP6200C
Circuit Breaker RB Cover (one position) - BCV
Cover Screws - 4020513002K
Meter Socket Cover (ringless type, one position) - MMRC
Pull Box Cover - MP56200PC
Line Phase and Neutral Lugs - MMLK500
Load Neutral and Service Ground Lugs Assembly: 7329704351 (includes connector and five lugs - used on the LEFT side of the pull box)
Load Neutral and Service Ground Lugs Assembly: 7329704353 (includes connector and three lugs - used on the RIGHT side of the pull box)
Mounting Screws: (1) 21427-20163 and (3) 2142717120 (needed for each assembly)
Equipment Ground Lugs Assembly: (2) 7329704451 (includes mounting bracket and three lugs - used on the LEFT and RIGHT side of the pull box)
Mounting Screws: (4) 2142217101 (2 required)
Parts Kit (one position, meter socket line side through tenant breaker base) - MP200KIT
Mounting Channel - 7329652101

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings