Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the T327NR, series E01 general duty safety switch?
Issue:
Repair parts

Product Line:
GD Safety Switch

Resolution:
The parts listed here are the only field replaceable parts.
Line base assembly - 4051051250
Load base assembly - 4051051150
Arc supressor - 4051057402
Neutral assembly - 4051050750
Base assembly mounting screws - 2142720241 (6 required for the line base and 7 for the load base)
Arc supressor mounting screw - 4020508201
Neutral bonding strap assembly - 4028331250
Neutral assembly mounting screw - 4020506501 (4 required)
Cross Arm Insulator - 4051030801 (insulator) and 4051031801 (dust shield - retainer for insulator)

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings