Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the DU324RB, series F1? (may be shown as F01)
Issue:
Repair parts

Product Line:
General Duty Safety Switch

Resolution:
The repair parts for the DU324RB, series F1 (F01) are as follows. No other parts are available.
Complete Line/Load Base (all one piece) - 4056703150 (requires one per switch - includes phenolic base, arc suppressors, lugs, rotor, switching blades, and fuse clips if applicable)
Complete Line/Load Base mounting screws - 40205-464-01 (requires 6 per line base)
Arc Suppressor Assembly - 40539-220-01(requires one per phase)
Arc Suppressor mounting screw - 40205-145-01
Lug Assembly - 40251-162-51 (per lug)
Lug Assembly mounting screw - 21401-222-40
Switch Mechanism - 40566-784-50 (also requires Interlock Shaft Gasket (40567-860-01)
Switch Mechanism mounting screws - 22999-405-62 (requires 2)
Handle Assembly - 40566-862-50 (requires handle gasket 40566-086-01)
Lockplate - 40566-857-01
Lockplate mounting screws - 22999-405-62 (requires 2)
Cover latch and spring - one each of 40566-072-01 (latch) and 40223-043-01 (spring)

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings