Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the H364DS, series F5? (may be shown as F05)
Issue:
What are the repair parts for the H364DS, series F5? (may be shown as F05)

Product Line:
Heavy Duty Safety Switch

Resolution:
The replacement parts for the H364DS, series F5 (F05) are as follows. No other parts are available.
Complete Line Base - 4056703550 (1 required; includes phynolic base, arc suppressors, lugs, rotor, switching blades, and fuse clips)
Line Base mounting screws - 4020514202 (6 required per line base)
Load Base Assembly - 4056678250 (1 required per phase; includes phynolic base, lugs, and fuse clips)
Load Base mounting screws - 4020514202 (2 required per load base)
Arc Suppressor Assembly - 4056677550 (1 required per phase)
Arc Suppressor mounting screw - 4020514501
Lug Assembly - CL20F (includes 6 lugs; requires mounting screws below)
Lug Assembly mounting screw - 2140122240 (per lug)
Switch Mechanism - 4056678650 (also requires mechanism coupling assembly 4056699850 and interlock connector assembly 4056718850)
Switch Mechanism mounting screws - 2194900001 (2 required)
Handle Assembly - 4056736850
Lockplate - 4056738901
Lockplate mounting screws - 2194900001 (2 required)

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings