Issue:
How is the HRK1020 installed in the safety switch?
Product Line:
Safety Switches
Resolution:
The HRK1020 consists of three rejection pins and collars. The rejection pin is inserted into a hole in the load side fuse clips. Once the rejection pin is inserted into the fuse clip, the collar is then pushed onto the rejection pin. A pair of pliers may be required to push the collar onto the rejection pin. The rejection pin should not be able to be removed once properly installed.
How is the HRK1020 installed in the safety switch?
Product Line:
Safety Switches
Resolution:
The HRK1020 consists of three rejection pins and collars. The rejection pin is inserted into a hole in the load side fuse clips. Once the rejection pin is inserted into the fuse clip, the collar is then pushed onto the rejection pin. A pair of pliers may be required to push the collar onto the rejection pin. The rejection pin should not be able to be removed once properly installed.
Released for: Schneider Electric USA