Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the available QO-SWN switch neutral breakers?
Issue:
Part numbers for QO-SWN breakers

Product Line:
Circuit Breakers

Resolution:
Most QO switch neutral breakers have gone obsolete. The ones that are still available are:
2 wire (1 hot, 1 neutral)
15 A - QO215SWN
20 A - QO220SWN

3 wire (2 hots, 1 neutral)
10 A - QO310SWN
20 A - QO320SWN
25 A - QO325SWN

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings