Issue:
Time Before Starting parameter in the ATS46, ATS48 and ATS480.
Product Line:
ATS46
ATS48
ATS480
Environment:
All series
Cause:
N/A
Resolution:
It is time delay after a STOP command in Freewheel mode or after the end of ramp or braking before a new START command will be accepted.
The default setting for tbS is 2 seconds.
During the time delay the display will show tbS.
If tbS is displayed it is an indication that the softstart detected the 24VDC was removed from the Stop terminal.
Time Before Starting parameter in the ATS46, ATS48 and ATS480.
Product Line:
ATS46
ATS48
ATS480
Environment:
All series
Cause:
N/A
Resolution:
It is time delay after a STOP command in Freewheel mode or after the end of ramp or braking before a new START command will be accepted.
The default setting for tbS is 2 seconds.
During the time delay the display will show tbS.
If tbS is displayed it is an indication that the softstart detected the 24VDC was removed from the Stop terminal.
Released for: Schneider Electric USA