Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can the ground fault feature be defeated for test purposes on the Masterpact NW circuit breaker?

Issue:
How do you disable the ground fault on a Masterpact breaker for primary injecting?

Product line:
Power Circuit Breakers

Resolution:
There are two ways to defeat ground fault on the NW breaker.  The handheld test kit or the full function test kit can both detect ground faults. If neither of these devices is available, then the "looping method" will have to be employed while primary injecting. See FA265488 for more information on the looping method.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings