Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the replacement control coil for the catalog number 9998SG*** E-Coil modification kit?
Issue:
9998SG*** E-Coil modification kit?

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
Type S Size 5 Starter

Resolution:
See replacement coil selection chart in the Class 9998 replacement coil section of current Digest. The E-Coil modification kit is designed to retrofit existing Class 8502/8536 Type SGO Series A device to Series B power plant. In no way should the Series B Coil be used with the other Series A power plant components.

Schneider Electric USA

Attachment(s)
Size 5 modification kits.PNG.png [147.14 KB]
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings