Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can an NF panel be supplied with a 250 A branch breaker option?
Issue:
Largest feeder

Product Line:
Panelboards

Resolution:
Yes, with a factory installed subfeed breaker or a merchandised subfeed breaker kit from the Online Digest. Note that the backbox or enclosure will change, as the subfeed branch is mounted in the end gutter opposite the panel mains and takes up quite a bit of mounting space in the gutter.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings