Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the standard lug for the legacy LC and LI circuit breaker?
Issue:
Standard lug for the LC and LI circuit breaker

Product Line:
Legacy Circuit Breaker

Resolution:
The standard lug is AL600LI5, which will accept (2) 4/0 AWG – 500 kcmil Al/Cu (1 lug per kit).

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings