Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Is there a longer extension for a 9007C54KC or 9007WKC ?
Consider a 9007J head with a Delrin rod extension. Possible products are:
9007JS2 18 inch rod, 9007JS5 36 inch rod, 9007JS4 25 inch rod, 9007JS6 13 inch rod, 9007JS7 8 inch rod, 9007JS9 12 5/8 inch rod. Alternative is the FA or LA lever. A third possibility is the adjustable lever using an S9 hub and the 9007R16 or R17 lever from the 9007F and FT line.


CTA-ID : 1608

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings