Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for a QMB325, Series D2 (D02)?
Issue:
Repair parts list for QMB325, series D2

Product Line:
QMB Switches

Resolution:
Only the parts listed below are considered field replaceable:
Arc Suppressor Assembly (2 per switch) - 4052031850
Arc Shield (2 per switch) - 4052085601
Load Base Assembly (2 per switch, includes lugs) - 4052112050
Load Base Mounting Screw (3 required per load base) - 2142720241
Load Base Side Insulator (1 per load base) - 4052098601
Handle Knob Kit - 4028343550
Lug Assembly (per lug) - 4025128750
Lug Mounting Nut (per lug) - 2342702400

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings