Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for an EZM114125, series M01 branch unit?

Issue:
Repair parts

Product Line:
EZM

Resolution:
Only the parts listed below are considered field replaceable:
Customer Cover (includes labels) - EZM114125C
Cover Screws - 4020513002K
Meter Socket Cover (cover for one-meter position) - MMC
Meter Socket Sealing Ring (aluminum latch type) - 2920910001
Parts Kit (one position, meter socket line side through tenant breaker base) - MM125KIT
Circuit Breaker RB Cover (one position) - BCV
Enclosure connecting hardware and Service Disconnect labels - 7329791750
Mounting Channel - 7329772301
Ground Bar - 73298-970-53
Mounting Bracket - 7329653201
Ground Bar Mounting Screws - (2) 2142217101
Bracket Mounting Screws - (2) 2153217161
End Closing Cap Kit - EZMCAP
End Closing Cap Kit (Right Side Only Shallow) - EZMSCAP
Top Endwall Rain Cap – 7329714601
Top Endwall Rain Cap Mounting Screws – 4020513002K (includes 10 screws; only 2 screws are used to secure the rain cap)

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings