Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for a QMB323TD, Series D2 (D02)?
Issue:
Previous Design Repair parts

Product Line:
QMB Branch Switches

Resolution:
The QMB device is a twin switch, meaning it contains two switches in the one device. Parts are listed per switch. Only the parts listed below are considered field replaceable:
Arc Shield/Suppressor Assembly - 4051239950 (1 required)
Load Base Assembly - 4052068050 (1 required; includes lugs)
Load Base Mounting Screw - 2142717161 (2 required per load base)
Handle Knob Kit - 4028343750

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings