Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for an EZM115125, Series M01 branch unit?
Issue:
Repair parts

Product Line:
EZM

Resolution:

Only the parts listed below are considered field replaceable:
Customer Cover - EZM115125C (includes labels)
Cover Screws - 4020513002K
Meter Socket Cover - MMC (one meter position)
Meter Socket Sealing Ring - 2920910001 (aluminum latch type)
Parts Kit - MM125KIT (one position; meter socket line side through tenant breaker base)
Circuit Breaker RB Cover - BCV (one position)
Enclosure connecting hardware and Service Disconnect labels - 7329791750
Mounting Channel - 7329772301
Ground Bar - 7329729750
Mounting Bracket - 7329653201
Ground Bar Mounting Screws - (2) 2142217101
Bracket Mounting Screws - (2) 2153217161
Top Endwall Rain Cap – 7329714601
Top Endwall Rain Cap Mounting Screws – 4020513002K (includes 10 screws; only 2 screws are used to secure the rain cap)
End Closing Cap Kit - EZMCAP
End Closing Cap Kit (Right Side) - EZMSCAP

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings